cancel
Showing results for 
Search instead for 
Did you mean: 

Check the STM32L011E4Y6TR peripheral circuit.

Tom.1
Associate

Is it a problem to set the constant of the external pull-up resistor connected to the "PB9_Boot0" signal to 100kΩ? (R13)

Also, if there is a problem with the connection, I would like you to point out the relevant part.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello @田�?� 智之​ and welcome to the Community :)

BOOT0/PB9 pin limitation: typical input leakage current = 2 µA and input frequency limited to 10 kHz (1.65 V < VDD < 2.7 V) and 5 MHz (2.7 V < VDD < 3.6 V).

I advise you to refer to RM0377 and the STM32L011x3/4 datasheet for more details about the electrical characteristics of the pull-up resistors. 

Check also the STM32L011xx/L021xx device errata, if you have same conditions.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen