2022-08-26 4:36 AM
I would like to use the STM32F779AI, in WLCSP package. I did not find any application notes, or schematics or dev board for such MCU.
Is there some litterature or example, schematics, ... talking about layout rules, VIAs, etc... for the WLCSP-180 (pitch 0.4mm) package.
Thanks in advance
Pascal
Solved! Go to Solution.
2022-08-29 1:43 AM
Hi @pazcal
Refer to this application note Getting started with STM32F7 Series MCU hardware development section 6.7 Recommendations for the WLCSP180 package then 8.5 WLCSP143 0.4 mm pitch design example
Also you can check the datasheet section 3 for more details about the pinout and package characteristics
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-26 9:41 AM
TBH I think the people you should start with are the PCBA guys you work with, they'll have a lot more insight into the board, stack-up, solder mask, and via-in-pad type stuff they can work with, and which PCB vendors do a good job of fill/planarization, etc.
2022-08-29 1:43 AM
Hi @pazcal
Refer to this application note Getting started with STM32F7 Series MCU hardware development section 6.7 Recommendations for the WLCSP180 package then 8.5 WLCSP143 0.4 mm pitch design example
Also you can check the datasheet section 3 for more details about the pinout and package characteristics
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-31 2:17 AM
Thanks for answer, but the question came from the PCBA Guys.
BR
paz
2022-08-31 2:17 AM
Thanks for your answer. The A.N will help
BR
paz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.