2025-02-06 8:47 AM
Hi,
STM32N6570-DK preloaded code works with the default MB1854B camera board. My question is:
"Does the default firmware support VD66GY?"
I tried and could not make it work.
When I switch the camera module to VD66GY S-BOARD, the LCD shows "Camera not detected, power off board, connect camera, power on board". I double checked my S-BOARD with STEVAL-EVK-U0I (PCB4405C) and it works fine. I also checked the FFC connection to make sure the TYPE B cable has to be used for my S-BOARD instead of TYPE A cable included in the DK kit.
Thanks,
Jimmy
2025-02-08 2:18 AM
Hello @JimmyW
Yes, the STM32N6570-DK out of the box example is designed to work with Sony IMX335 camera sensor is a 5 Mega Pixels (MB1854B) and cannot support VD66GY.
Best regards,
Romain
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.