cancel
Showing results for 
Search instead for 
Did you mean: 

Am working on NUCLEO STM32F401RE , so after debugging the code, am facing this issue. Please advise for this, so i can work speedy. Target no device found Error in initializing ST-LINK device. Reason: No device found on target.

kabid.1
Associate

STMicroelectronics ST-LINK GDB server. Version 7.0.0

Copyright (c) 2022, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Target no device found

Error in initializing ST-LINK device.

Reason: No device found on target.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hallo @kabid.1​ ,

I advise you to refer to this FAQ: How to solve debugger connection issues.

Check if all jumpers are correctly configured.

Try using latest release of STM32Cubeprogrammer, and make sure to upgrade the ST-LINK/V2-1 firmware.

Try connect to "Under reset" mode.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen