cancel
Showing results for 
Search instead for 
Did you mean: 

help STM32-P103 RS232

mustapha_menhou
Associate II
Posted on March 25, 2013 at 22:18

Hi i

 would like

to use the circuit

MAX3232

(

RS232

adapter

) to connect two 

PORT

RS232

with this

 circuit 

using just

TX and RX

only

if possible

this experience?

?

?

?

?

and thank you 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on March 25, 2013 at 23:02

There seems to be a language barrier here. Perhaps it would be easier to explain your requirement with a diagram...?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mustapha_menhou
Associate II
Posted on March 26, 2013 at 00:15

Here is a

PDF

that

represents

my problem

if

possible to do this

configuration?

??

________________

Attachments :

Doc1.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1An&d=%2Fa%2F0X0000000bjO%2FMxvFcOji_FYohzLHw5WB39F3L3WIkazQ.unp2P0.vmY&asPdf=false
Posted on March 26, 2013 at 07:47

By ''STM32-P103'' I assume you mean this:

https://www.olimex.com/Products/ARM/ST/STM32-P103/

Note that it has one RS232 port already - so you only need to add one other.

Study the documentation to see where the other UART port pins can be accessed on the various connectors on the board...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on March 26, 2013 at 09:31

I see you have also posted the same question in a different thread:

/519d41ef

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.