2024-09-30 8:24 AM - last edited on 2024-09-30 8:44 AM by Andrew Neil
what is A/D register for? when i bring the st25r tag(sticker one) near the st25 nfc its value changes. And how is interrupt generated? what are the values of registers to be set in order to read a NfC tag?pseudo code for it.
Solved! Go to Solution.
2024-09-30 11:36 PM
Hi sanjogsakota,
please check the DS, there are a number of direct commands which trigger an A/D conversion and put the result into the mentioned register.
BR, Ulysses
2024-09-30 2:26 PM
Hi Sanjog,
which product do you refer to? ST25R3916?ST25R3916B?ST25R3911?
Rgds
BT
2024-09-30 7:02 PM
i am using ST25R3911B -DISCO but using an external stm32(blue pill)
2024-09-30 11:36 PM
Hi sanjogsakota,
please check the DS, there are a number of direct commands which trigger an A/D conversion and put the result into the mentioned register.
BR, Ulysses