2014-02-24 08:02 AM
Hi all,
I can see in the documentation the command ''Lock Sector'' and used in the android demo application but I cannot figure how to unlock a sector. Using the application, I have changed the first password and locked the first sector and now I cannot write it and unlockit. Can Anybody help me?Thanks a lot. #lock-sector #m24lr #password2014-02-25 12:54 AM
Ok, I see how to unlock a sector, the problem is that the first password has been changed and I don't know its value. Anybody knows any way of resetting its value?
is the device that I have. Thanks a lot!2014-03-05 12:48 AM
Hello,
On delivery,
the three default password values are set to 0000 0000h and are activated.
When a sector is locked , you must present the correct password to unlock it , access is then define by SSS setting .
The I2C password is a Super user password and allow to overwrite the RF password and SSS which is not possible in RF for security purpose .
Have a nice day,
ST NFC/RFID Dynamic tad e2e support2014-11-24 05:10 AM
Hello,
I have read in M24LR64E that RF password can not be read or write from I2C.(Datasheet M24LR64E-R page 31/140 --> ''The next three 32-bit blocks store the three RF passwords. These passwords are neither read- nor write- accessible in the I2C mode.
''Could you confirm that it's possible to read/change/reset the RF password from I2C?Regards,Dom