2019-03-07 8:47 AM
I want to tune the Cin, Clen and Cout variable caps on the ST25RU3993 Eval kit. I have modified the Evaluation kit to use a different micro controller, however im using the same source code with very minor modification (to suit the pins that I am using on my micro). When I set capacitor values I then call the GetReflectedPower function which in turn calls the GetADC. However my ADC seems to always return 0. Am I missing something with the hardware set up? I have attached a code sample for clarity.
Solved! Go to Solution.
2019-03-07 9:25 AM
I think I have solved the problem it seems in my main software I have moved the antenna initialise function, and as such it was never being called. WIth this enabled, I now received ADC values.
2019-03-07 8:56 AM
I should add its the ST25Ru3993 evaluation board that I am using.
2019-03-07 9:25 AM
I think I have solved the problem it seems in my main software I have moved the antenna initialise function, and as such it was never being called. WIth this enabled, I now received ADC values.
2019-03-13 2:39 AM
Hello Chris,
So far I haven't reviewed the code you have sent, but have you checked to turn ON the RF power prior the call to measure the reflected power?
Cheers,
B
2019-03-14 2:02 AM
Hi Bart,
As mentioned in my post above it seems I hadn't, as I had moved the antenna initialise function.
It seems now to be working.
Chris