cancel
Showing results for 
Search instead for 
Did you mean: 

What is the PLL lock time for the ST25RU3993?

kyle.tingey
Associate

When trying to frequency hop on the main PLL, I observe a lock time of ~150ms. This seems quite high and I can't find any more information in the datasheet on the matter. Is anyone able to verify the PLL lock time?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bart Herse
Senior II

Hello,

In case the PLL is already locked to a certain frequency re-locking to a new frequency depends on the frequency and the frequency hopping step, nevertheless the locking time should be below 500µs.

For start-up the locking time is longer and again depending on the target frequency. Expect a locking time around 800µs.

All above is concerning cases at which the VCO segment is manually chosen.

In case a procedure which is using the Automatic VCO Range Selection (A4h) command is implemented, then the overall locking time is longer since the command A4h itself is taking up to 6 ms to complete, reporting the optimal VCO segment.

Cheers,

B

View solution in original post

1 REPLY 1
Bart Herse
Senior II

Hello,

In case the PLL is already locked to a certain frequency re-locking to a new frequency depends on the frequency and the frequency hopping step, nevertheless the locking time should be below 500µs.

For start-up the locking time is longer and again depending on the target frequency. Expect a locking time around 800µs.

All above is concerning cases at which the VCO segment is manually chosen.

In case a procedure which is using the Automatic VCO Range Selection (A4h) command is implemented, then the overall locking time is longer since the command A4h itself is taking up to 6 ms to complete, reporting the optimal VCO segment.

Cheers,

B