cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R95: DATA Read and Write problem ISO1443A

NM
Associate III

0693W00000DnYRMQA3.jpgHi,

I am getting the UUID of the device but I am unable to read or write the data. Its giving the response of 0x87 00 (No Tag). Help me to solve the problem... How to read the data from the memory...?

Please check out the above commands sets...

Board: X-Nucleo-NFC-03A1

Kind Regards,

Nishanth M

11 REPLIES 11

Hi,

Thanks for the reply.

Now I can read and write the data with different type but same manufacturer such as MIFARE Ultralight & NTAG213/215/216.

Still I am trying to read & Write with the Mifare Classic 1K.

I want your suggestion such that in my PCB layout, I am trying to put all the RF chip and components will be at center of the antenna. So that I can get more space. If I seen the CR95 Eval board the antenna part is separate and no other components also placed at the bottom and inside the antennal tracks.

0693W00000DnjeWQAR.jpgThis above type of placement is recommended?

Will you share the PCB guidelines for the CR95H...

Kind Regards,

Nishanth M

Brian TIDAL
ST Employee

Hi,

in accordance with this Community Ground Rules, I would suggest to start a new thread regarding the PCB and HW related questions and to mark this current thread as replied.

Thanks in advance,

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.