2023-12-15 5:39 AM - edited 2023-12-15 5:55 AM
Hello,
I'm using RFAL v2.6.0 and ST25R3911B and I get an issue with the IRQ management.
Using ISO14443 Type-A tag, the IRQ remains high causing the while loop not to exit.
In this condition, the i_err bit of the main interrupt register is '1' while the two interrupt registers (Timer and NFC interrupt register and Error and wake-up interrupt register) have all of their bits to '0'.
Reading these register in a loop cannot clear the i_err bit.
The last content prior the lock state is:
- Main interrupt register: 0x33 -> i_rxs, i_rxe, i_tim, i_err
- Timer and NFC interrupt register: 0x20
- Error and wake-up interrupt register: 00 (Should be different from 0)
2023-12-18 1:21 AM
Hi Ulysses,
Yes, you are right.
But trying first this condition, I also see other rarer cases where the iregs[2] was not null (as expected, with a crc error for instance) and reading the registers does not success to clear the main register too. Only iregs[2] was cleared by the read operation.
I will send you traces if I can get them one day :)
Regards,
Frederic
2024-01-02 4:55 AM
Hi Ulysses,
First, may the New Year bring you everything you wish.
I get another issue with the code above when trying to use rfalT2PollerWrite function. It always results in CRC error.
I try to trace the IRQ registers when I send the command and I get the following sequences :
With my final code (no condition on iregs[2])
I (68421) DEBUG: (HEAP:171052) (1704198943:194265000) [fart_scan.c:166] Found tag: 0414
I (68441) DEBUG: (HEAP:171052) (1704198943:208944000) [st25r3911_interrupt.c:119] 08, 00, 00
I (68441) DEBUG: (HEAP:171052) (1704198943:213070000) [st25r3911_interrupt.c:119] 31, 00, 80
I (68451) TRACE: (HEAP:171052) (1704198943:220982000) [rfid.c:567] [MSL-RFID] Rfal error (T2 write), sts=21
With your proposal (condition iregs[2] == 0) I get a lock into the while loop
I (57131) DEBUG: (HEAP:171048) (1704199559:580346000) [st25r3911_interrupt.c:119] 32, 20, 00
I (57141) DEBUG: (HEAP:171000) (1704199559:589881000) [fart_scan.c:166] Found tag: 0414
I (57151) DEBUG: (HEAP:171000) (1704199559:604509000) [st25r3911_interrupt.c:119] 08, 00, 00
I (57161) DEBUG: (HEAP:171000) (1704199559:608634000) [st25r3911_interrupt.c:119] 31, 00, 80
I (57161) DEBUG: (HEAP:171000) (1704199559:616370000) [st25r3911_interrupt.c:119] 03, 20, 80
I (57171) DEBUG: (HEAP:171000) (1704199559:625484000) [st25r3911_interrupt.c:119] 01, 00, 80
I (57181) DEBUG: (HEAP:171000) (1704199559:634599000) [st25r3911_interrupt.c:119] 01, 00, 80
I (57191) DEBUG: (HEAP:171000) (1704199559:643715000) [st25r3911_interrupt.c:119] 01, 00, 80
...
Removing the while condition (and no extra code to clear the register), it works and I get the following:
I (60701) DEBUG: (HEAP:171180) (1704197378:880586000) [fart_scan.c:166] Found tag: 0414
I (60711) DEBUG: (HEAP:171180) (1704197378:895260000) [st25r3911_interrupt.c:119] 08, 00, 00
I (60721) DEBUG: (HEAP:171180) (1704197378:899392000) [st25r3911_interrupt.c:119] 31, 00, 80
I (60721) DEBUG: (HEAP:171180) (1704197378:907161000) [st25r3911_interrupt.c:119] 03, 20, 80
As far I understand the CRC error may be expected for Type 2 operation as ack/nack are on 4 bits only. The fix we made is so not correct as we lost the fifo content in this case. Any ideas ?
2024-01-02 8:45 AM
Hi Frederic,
the 4-bits ACK/NACK in type 2 causes an I_crc and/or an I_par interrupt that is internally converted into an RFAL_ERR_INCOMPLETE_BYTE return code. The rfalT2TPollerWrite function then checks that this incomplete byte is an ACK. Thus, having an I_crc is an expected behavior in case of 4 bits ACK/NACK reception.
It would really be helpful to have an SPI trace (CLK/MISO/MOSI/CS+ ST25R3911B_IRQ) to better understand your issue.
Some additional questions:
Rgds
BT
2024-01-03 12:14 AM - edited 2024-01-03 12:50 AM
Hello Brian,
As I said before unfortunately I do not have any advanced scope to get the SPI trace. And there is no test point on the custom board. I only have total Phase beagle. If I have time I will try to get data.
- We are using ST25R3911B or ST253916 for 3 years now on different custom board versions.
We always had a problem with the while loop in the RFAL (for NFC Type 2 tags). The only way to get the library worked was to remove the while loop.
On the last firmware version I decided to remove the IRQ management that can be problematic on espressif and use polling. I still have the same issue with NFC Type 2 tags.
- Vdd is 5V.
- Vdd_io is 3.3V.
- The board is powered by the mains (12V then two stages regularor, plus CMCC filter).
Regards,
Fred
2024-01-05 1:37 AM - edited 2024-01-05 1:38 AM
Dear Fred,
This behavior is not known and the only efficient way to proceed is to retrieve a SPI trace (incl IRQ line) of the occurrence, so that we can perform technical analysis.
Meanwhile let me share some additional details:
Hope it helps
We look forward for a SPI trace of the occurrence.
Kind regards
GP
2024-01-05 3:02 AM
Hi Gregory,
Thanks for the information.
Yes we are using the right configuration. And CS is hardware managed.
As I discussed with Brian in private message, I can imagine we have some violation in SPI. Why not ?
But it cannot explain why we are not able to recover by sending another read.
Because how can you explain that the read operations works 95% of time and when the issue occured, it was impossible to clear the status by reading the register for ever. And at the same time sending other commands through SPI (such as clear command) works fine. It means SPI is not stuck and so one of the reading operation should succeed to clear the register.
My feeling (maybe I'm wrong) is we are not looking on the right point. I have been working in ST, Atmel, Inside and Starchip companies for a long time and it looks more at a rare timing race issue in HW.
Whatever, I will send SPI traces as soon as possible.
Regards,
Frederic
2024-01-08 1:18 AM
Hi,
I am reading down there about TotalPhase Beagle. It looks like only providing the data packets plus timings not no waveforms.
We have often seen issues only in the waveforms so a logic analyzer is typically superior for this use case. If possible try to get one as well.
BR, Ulysses