cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3911B-DISCO - activating specific UID

Ralphie
Visitor

I'm trying out the ST25R3911B-DISCO board to evaluate how to read data from multiple 14443A RFID tags. Under the Polling tab I can see all the UIDs for the tags near the board.  However, when I go over to the NFC Type 2 tab, if I select "Configuration" and then "WUPA->Active", the UID field will always be filled by a particular UID.  I can read data from that tag just fine.  How can I activate the other tags so I can read the data on them?  I tried typing a different UID from a nearby tag into the UID field but that just gets overwritten when I click on "WUPA->Active".  

Is it possible to individually read data from any tag that shows up in the Polling scan?

Thanks

-R

0 REPLIES 0