2020-11-02 3:47 PM
Hi there
It seems that ST25DV64K-IER6S3 does not load the I2C bus even when there is no power on VCC. I have checked the datasheet but I have not found any information on that.
Could you confirm it?
BR
Gilberto
Solved! Go to Solution.
2020-11-03 2:44 AM
Hello Gilberto,
Yes, no problem with that.
The I2C outputs of ST25DV are open drain. This means they can only drive the signal low, and they can only drive it low when the VCC is active. With VCC=0, they will simply stays Hi-Z, not perturbating other i2c slaves.
Best regards.
2020-11-03 12:29 AM
Hello,
What do you mean exactly by "load the bus" ?
If the question is "is I2C active when vcc=0", the answer is no.
Best regards.
2020-11-03 2:04 AM
Hi
The i2c bus has an accelerometer, an st25dv and a temperature sensor on it . Can the cpu communicate with these others devices when the ST25DV vcc is 0?
BR
Gilberto
2020-11-03 2:44 AM
Hello Gilberto,
Yes, no problem with that.
The I2C outputs of ST25DV are open drain. This means they can only drive the signal low, and they can only drive it low when the VCC is active. With VCC=0, they will simply stays Hi-Z, not perturbating other i2c slaves.
Best regards.