2019-10-18 1:43 AM
Hello,
I have bought an ST25DV Discovery kit but it cannot be used with the ST25PC software, it says that the IC does not support *** feature.
Hint: when I read the UUID, I have Hitashi as manufacturer (byte 2 is 0x03 instead of 0x02 as indicated in the datasheet).
[DEBUG] FC
[DEBUG] 67
[DEBUG] FB
[DEBUG] 4
[DEBUG] 0
[DEBUG] 25
[DEBUG] 3
[DEBUG] E0
Do you know what's going on?
2019-10-18 5:49 AM
Hi Anthony,
could you please say if you read the same UID from another application (Phone app for example) ?
Thank you,
Damien
2019-10-18 6:51 AM
Yes absolutely, I can read the same with the NXP RFID tool on Android (and it also says that it comes from Hitachi). Looks like the ST25DV is not an ST design :)
2019-10-22 7:23 AM
Dear Anthony,
Yes this value of IC manufacturer code is not correct.
Is it possible to tell us the origin of this ST25DV discovery board ? Where and when did you acquire it ?
This would help to understand what's going one.
Thank you and best regards.
2019-10-22 7:57 AM
Yes, we bought it on Farnell on 5 sept. 2019
Réf.Farnell France : 70042712
Date de la commande :5 sept. 2019
https://fr.farnell.com/stmicroelectronics/st25dv-discovery/kit-de-decouverte-tag-nfc-rfid/dp/2761534
2019-12-11 9:02 AM
Hi,
Do you have any clue on that point?
Regards,
Anthony
2019-12-17 6:31 AM
Hello Anthony,
I have contacted you by private message on this topic 2 months ago, proposing you that you send back to ST the defective part for analysis. Did you see this message and did you sent anything ?
Best regards.