2021-09-01 3:42 AM
Hello, I accidentally connected Vcc to the interrupt pin in an X-NUCLEO-NFC06A1, now I don't get any interrupts. Is it terminally burnt or can I configure an IRQ from somewhere else on the board?
Solved! Go to Solution.
2021-09-01 4:09 AM
The interrupt pin of the X-NUCLEO-NFC06A1 is connected to pin IRQ of the ST25R3916, which is an output, most likely destroyed and no chance to get the IRQ from somewhere else.
The only possibilities: replace the ST25R3916 or get a new X-NUCLEO-NFC06A1.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
Good luck!
/Peter
2021-09-01 4:09 AM
The interrupt pin of the X-NUCLEO-NFC06A1 is connected to pin IRQ of the ST25R3916, which is an output, most likely destroyed and no chance to get the IRQ from somewhere else.
The only possibilities: replace the ST25R3916 or get a new X-NUCLEO-NFC06A1.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
Good luck!
/Peter