2024-10-17 8:13 AM
Hi All,
I having been using the st25R3911B-disco board for the past several months as a development tool for a project using the ST25DV chipset. Up until now I have really only had to use the iso15693writ/readblockblock functions that I saw in the cpp example project. Now however I need to write to and read from special registers on the tag i am communicating with, such as the dynamic registers on the ST25DV chip. Its not obvious to me which functions from ST25R3911B header file I need to use to do this, can someone point me in the right direction?
Thanks,
Patrick
Solved! Go to Solution.
2024-10-17 8:33 AM
Hi Patrick,
iso15693TxRxNBytes function can be used to send custom commands such as Read Configuration or Read Dynamic Configuration to a ISO15693 tag. Just format the content of your buffer according to the command specification in the tag datasheet and then sent it with iso15693TxRxNBytes.
See also https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/can-i-have-some-guidance-on-how-to-use-the-str25r3111discocomm/td-p/91335 and other post on this community related to iso15693TxRxNBytes.
Rgds
BT
2024-10-17 8:33 AM
Hi Patrick,
iso15693TxRxNBytes function can be used to send custom commands such as Read Configuration or Read Dynamic Configuration to a ISO15693 tag. Just format the content of your buffer according to the command specification in the tag datasheet and then sent it with iso15693TxRxNBytes.
See also https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/can-i-have-some-guidance-on-how-to-use-the-str25r3111discocomm/td-p/91335 and other post on this community related to iso15693TxRxNBytes.
Rgds
BT