cancel
Showing results for 
Search instead for 
Did you mean: 

Reading ST25TA02K tags

MDubo.1
Associate

Hi

I'm using the ST25R3916 IC to read/write the data of the tags from the ST25-TAG-BAG-E. What sequence do I need to use to read the user data?

regards

Matties

1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi Matties,

X-CUBE-NFC6 contains a demo project with a configuration ....PollingTagDetectNDEF which shows reading, writing NDEF from a T4T and formatting of ST25TA tags as T4T.

You are not bound to use NDEF for these tags so you can also just pick the commands from this demo and reassemble them to your needs.

Regards, Ulysses

View solution in original post

1 REPLY 1
Ulysses HERNIOSUS
ST Employee

Hi Matties,

X-CUBE-NFC6 contains a demo project with a configuration ....PollingTagDetectNDEF which shows reading, writing NDEF from a T4T and formatting of ST25TA tags as T4T.

You are not bound to use NDEF for these tags so you can also just pick the commands from this demo and reassemble them to your needs.

Regards, Ulysses