Skip to main content
FurkanSenol
Associate II
Oct 26, 2022 6:33 AM UTC
Solved

Reading NFC tags that are in phone case

Hello,

We are able to detect and read NFC tags with ST25R3920, but we have a little problem. When we are trying to read an NFC tag that is in a phone case (credit card, ID card etc.) we can't get a reading at all. Our first guess was that mobile phone is creating a field that interferes with NFC. Could there be something wrong or different in our software to get a reading like this? Should I be doing different configurations on registers like Antenna calibration, External Field Detector Threshold? What are your suggestions for this case?

Thanks in advance!

Best regards,

Furkan

    This topic has been closed for replies.
    Travis Palmer
    Travis PalmerBest answer
    ST Employee
    Nov 3, 2022 8:05 AM UTC

    Hello Furkan,

    Because of the close proximity of the card and phone, the phone is changing the resonance frequency of the card.

    As example in free air the card is tuned to 14.2MHz. When beeing put in the case of the resonance increases to something like 19MHz. This effect is due to metal parts inside the phone.

    This is affecting the power transfer between reader and card. The card will receive less power and can therefore not be read successfully.

    Also the readers antenna geometry can play a role here.

    Since you said, that the NFC06A1 can read the card in this condition, it should be also possible to read it with your device.

    AAT (antenna tuning) can be a great help here, but can also make it a bit more complicated.

    I would recommend to measure the smith chart of the reader in free air and 1cm distance to the card in the case.

    If you are using AAT (like on the default NFC06A1) you have to power the board and disable the driver (Register 27h set to 0xXF => bit d_res =0xF).

    If no AAT is used, the board can simply left unpowered.

    The above mentioned application notes can be a great help to increase the output power of your device.

    Please feel free to share your custom antenna design (including antenna parameters) as well as the above mentioned smith charts.

    br Travis

    5 replies

    Brian TIDAL
    ST Technical Moderator
    Oct 26, 2022 7:35 AM UTC

    Hi,

    my guess is that the phone case has an anti RFID card holder. Just remove the phone from its case and try to read the tag in the phone case: if you can't read it, this means that the phone case has an anti RFID shield.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    FurkanSenol
    Associate II
    Oct 26, 2022 10:40 AM UTC

    Hello Brian,

    We can read the tag when we remove the phone from it's case. In fact we can read the tag with X-NUCLEO-NFC06A1 shield on NUCLEO-L476RG board when phone is in the case. We just can't read it with our custom board. I should have mentioned this earlier, sorry for the lack of information.

    Could it be caused by antenna design faults?

    Brian TIDAL
    ST Technical Moderator
    Oct 26, 2022 11:51 AM UTC

    Hi,

    ST provides several application notes and tools to help customer to design and to verify their board.

    Application notes:

    Tools

    Chapter 7 of AN5276 provides guidelines for Design verification. This can be an entry point for your investigation.

    Let us know whether more support on this issue is needed.

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    FurkanSenol
    Associate II
    Oct 26, 2022 12:54 PM UTC

    Hello Brian,

    Thanks for all the information! I will get help from hardware team and try to diagnose problem. I will post here if we find the problem and the solution to fix it.

    Best regards,

    Furkan

    Travis Palmer
    Travis PalmerBest answer
    ST Employee
    Nov 3, 2022 8:05 AM UTC

    Hello Furkan,

    Because of the close proximity of the card and phone, the phone is changing the resonance frequency of the card.

    As example in free air the card is tuned to 14.2MHz. When beeing put in the case of the resonance increases to something like 19MHz. This effect is due to metal parts inside the phone.

    This is affecting the power transfer between reader and card. The card will receive less power and can therefore not be read successfully.

    Also the readers antenna geometry can play a role here.

    Since you said, that the NFC06A1 can read the card in this condition, it should be also possible to read it with your device.

    AAT (antenna tuning) can be a great help here, but can also make it a bit more complicated.

    I would recommend to measure the smith chart of the reader in free air and 1cm distance to the card in the case.

    If you are using AAT (like on the default NFC06A1) you have to power the board and disable the driver (Register 27h set to 0xXF => bit d_res =0xF).

    If no AAT is used, the board can simply left unpowered.

    The above mentioned application notes can be a great help to increase the output power of your device.

    Please feel free to share your custom antenna design (including antenna parameters) as well as the above mentioned smith charts.

    br Travis