2015-12-07 04:22 PM
The default configuration has 1 NDEF file that occupies the entire memory. Is it possible to slice up the memory between 2 or more NDEF files? If more than one file can be created, what is the maximum number of files that on tag can accommodate? Is that 15 (inferred from SELECT command)?
#ndef-st25ta64kSolved! Go to Solution.
2016-02-26 01:57 AM
Dear Don,
YOur understanding is correct. With ST25TA64K product you have to use NDEF file structure, memory cannot be adressed directly. Best Regards, NFC Product support12015-12-11 06:13 AM
Dear Sibi,
ST25TA64K supports only 1 NDEF file. Could I ask you for which application you need more than 1 NDEF file ? Could several NDEF records be used within the NDEF file in your case ? Best Regards, NFC Product support12016-02-23 07:51 AM
Is it possible to use the ST25TA64K as just memory, i.e. not used NDEF at all ?
We need to store a small amount of binary data, but don't need NDEF. However, I don't see anything in thge ST25XXX data sheets that indicate this is possible, and that use of NDEF is mandatory for this series of RFID tags. Is this correct ?2016-02-26 01:57 AM
Dear Don,
YOur understanding is correct. With ST25TA64K product you have to use NDEF file structure, memory cannot be adressed directly. Best Regards, NFC Product support1