cancel
Showing results for 
Search instead for 
Did you mean: 

NFC Tap app transfer data using the FTM mailbox feature

NDvas.3
Associate III

Hey Guys,

I am trying to use the NFC Tap app to transfer data to an ST25DV device I have here, using the FTM mailbox feature.

Mailbox is enabled. I get an error message from the App saying the send had failed.

General question: When the App sends over the data to the device, do I have to read it in that moment or in fact, do I have to do anything at all or does the ST25 takes care of this for me and I just need to know when the transfer is over and read the mailbox's content?

If there is someone here who is working with this and can shade some light on this for me it would be great.

Thank you,

Nir

10 REPLIES 10
France Berthelot
ST Employee

Hello

There is several SE generations, if NFC is available not only for Payment , the answer is yes. If you can R/W tag , MB features should work too.

FB