cancel
Showing results for 
Search instead for 
Did you mean: 

NFC readers with I2C or UART interface.

MBlac.2
Associate

We would prefer to not use SPI to interface to a NFC reader as we are I/O and peripheral constrained here.

I didn't see I2C as an option for any of the ST25R95, ST25R3911B or CR95HF. UART is an option for the CR95HF, but it is not available for it's successor product the ST25R95.

So our interface requirements are steering us towards the CR95HF. Is that my best choice here?

1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

see https://community.st.com/s/question/0D53W00000Bsjx4SAB/differences-between-st95hf-and-st25r95 for the differences between  CR95HF, ST95HF and ST25R95. In particular "For new developments, it is recommended to use the ST25R95. CR95HF can still be ordered for existing developments or for developments based on UART communication." The X-CUBE-NFC3 package supports the UART (see https://community.st.com/s/question/0D50X0000B7YwL7SQK/how-to-use-uart-interface-instead-of-spi-with-xnucleonfc03a1-and-xcubenfc3-polling-demo).

Note that the ST25R3916B supports the I2C.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

Hi,

see https://community.st.com/s/question/0D53W00000Bsjx4SAB/differences-between-st95hf-and-st25r95 for the differences between  CR95HF, ST95HF and ST25R95. In particular "For new developments, it is recommended to use the ST25R95. CR95HF can still be ordered for existing developments or for developments based on UART communication." The X-CUBE-NFC3 package supports the UART (see https://community.st.com/s/question/0D50X0000B7YwL7SQK/how-to-use-uart-interface-instead-of-spi-with-xnucleonfc03a1-and-xcubenfc3-polling-demo).

Note that the ST25R3916B supports the I2C.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.