2018-02-28 1:28 PM
I would like to measure the current consumption during the 'Wake-up' mode with capacitive or inductive sense, and also during the active rf-reads. Currently, the chip is powered by 5V and 3.3V. I am thinking to remove the 5V source and connect the Vdd to 3.3V as well. I can monitor the current coming from the 3.3V source. I should also remove the power LED to eliminate the current draw.
Anything else I am missing?
Solved! Go to Solution.
2018-03-05 11:54 PM
Hi Joseph,
This sounds like a good plan.
Please be aware that pin 2 and 4 of CN6 are both connected to 3.3V plane and that the power consumption in inductive wake-up and HF-field-on (
active rf-reads)
will be different/lower if the chip is supplied via 3.3V instead of 5V.BR Travis
2018-03-05 11:54 PM
Hi Joseph,
This sounds like a good plan.
Please be aware that pin 2 and 4 of CN6 are both connected to 3.3V plane and that the power consumption in inductive wake-up and HF-field-on (
active rf-reads)
will be different/lower if the chip is supplied via 3.3V instead of 5V.BR Travis
2018-03-19 9:38 AM
Hi Travis,
I made the changes as described and disconnect pin 2 on CN6. I then programmed the wake-up Timer Control Register (31h) with a value of 0 in order to observe the wake-up current. When I measure the current through the 3V3 line, I got 5.5µA, but the datasheet says 3.6µA. How can I get closer to that value?
Thanks.
P.S. I am using the demo firmware from
2018-03-22 3:18 AM
Dear Joseph
Can you please confirm that the oscilator and mcu_clk is not turned on?
And the following conditions are fullfilled?
Which kind of amp-meter have you used?
The values for this mode would be 1.6µA min, 3.6µA typical and 8µA max.
BR Travis