2014-05-14 6:03 AM
Hello,
I wish to use the M24LR16E as a NFC tag. In order to do this I have an ANT1-M24LR16E, a CR95HF and an Aardvark for the I2C communication.With the M24LRxx_Application_Software I send a text through the RF (with the CR95HF) and then I am trying to change this text through the I2C with the Aardvark.The batch code below:<aardvark> <configure i2c=''1'' spi=''0'' gpio=''0'' tpower=''1'' pullups=''1''/> <i2c_bitrate khz=''400''/> <i2c_write addr=''0x53'' count=''2'' radix=''16'' > 00 00</i2c_write> <i2c_write addr=''0x53'' count=''4'' radix=''16'' > E1 40 FF 05 </i2c_write> <i2c_write addr=''0x53'' count=''4'' radix=''16'' > 03 09 D1 01</i2c_write> <i2c_write addr=''0x53'' count=''4'' radix=''16'' > 05 54 02 65</i2c_write> <i2c_write addr=''0x53'' count=''4'' radix=''16'' > 6E 64 61 FE</i2c_write> <i2c_write addr=''0x53'' count=''2'' radix=''16'' > 00 00</i2c_write> <i2c_read addr=''0x53'' count=''16''/></aardvark>The bytes read by the Aardvark(I2C) are the ones previously written through the RF.I don't seem to be able to change them. Can you tell me if there is more to the I2C protocol that I missed in the datasheet?
Best regards, Adina #m24lr #m24lr #m24lr-read-write-problem #m24lr16e #aardvakSolved! Go to Solution.
2014-05-16 5:16 AM
Hi Adina,
Regarding the batch code and how parameters are sent to the Aardkvard reader, I suspect a mistake in your programming sequence :
For read sequence, your batch code shows :
<i2c_write addr=''0x53'' count=''2'' radix=''16'' > 00 00</i2c_write>
<i2c_read addr=''0x53'' count=''16''/>That means the reader send :
START + 0xA6 + 0x00 + 0x00 STOP (it could be better NOT to send STOP Here) + START+ 0xA7 + read 16 bytes
Where A7 is device select for a send command, 00 00 is address 0xA6 is device select for a receive data command
This is Ok and can work. If you have a way to avoid sending te STOP at the end of the first
<i2c_write add>
it could be better.
For write sequence, your bach code shows :
<i2c_write addr=''0x53'' count=''2'' radix=''16'' > 00 00</i2c_write>
<i2c_write addr=''0x53'' count=''4'' radix=''16'' > E1 40 FF 05 </i2c_write>That means the reader send :
START + 0xA6 + 00 + 00 + STOP + START+ 0xA6 + E1 + 40 + FF + 05 + STOP
That is not compliant with I2C write sequence described in the datasheet
To be able to write E1 40 FF 05 at address 00 00 , you need to send :
START + 0xA6 + 00 + 00 E1 40 FF 05 STOP
That could be :
<i2c_write addr=''0x53'' count=''6'' radix=''16'' > 00 00 E1 40 FF 05 </i2c_write>
<i2c_write addr=''0x53'' count=''6'' radix=''16'' > 00 04 03 09 D1 01</i2c_write> <i2c_write addr=''0x53'' count=''6'' radix=''16'' > 00 08 05 54 02 65</i2c_write> <i2c_write addr=''0x53'' count=''6'' radix=''16'' > 00 0C 6E 64 61 FE</i2c_write>I hope this will solve the issue
2014-05-16 5:16 AM
Hi Adina,
Regarding the batch code and how parameters are sent to the Aardkvard reader, I suspect a mistake in your programming sequence :
For read sequence, your batch code shows :
<i2c_write addr=''0x53'' count=''2'' radix=''16'' > 00 00</i2c_write>
<i2c_read addr=''0x53'' count=''16''/>That means the reader send :
START + 0xA6 + 0x00 + 0x00 STOP (it could be better NOT to send STOP Here) + START+ 0xA7 + read 16 bytes
Where A7 is device select for a send command, 00 00 is address 0xA6 is device select for a receive data command
This is Ok and can work. If you have a way to avoid sending te STOP at the end of the first
<i2c_write add>
it could be better.
For write sequence, your bach code shows :
<i2c_write addr=''0x53'' count=''2'' radix=''16'' > 00 00</i2c_write>
<i2c_write addr=''0x53'' count=''4'' radix=''16'' > E1 40 FF 05 </i2c_write>That means the reader send :
START + 0xA6 + 00 + 00 + STOP + START+ 0xA6 + E1 + 40 + FF + 05 + STOP
That is not compliant with I2C write sequence described in the datasheet
To be able to write E1 40 FF 05 at address 00 00 , you need to send :
START + 0xA6 + 00 + 00 E1 40 FF 05 STOP
That could be :
<i2c_write addr=''0x53'' count=''6'' radix=''16'' > 00 00 E1 40 FF 05 </i2c_write>
<i2c_write addr=''0x53'' count=''6'' radix=''16'' > 00 04 03 09 D1 01</i2c_write> <i2c_write addr=''0x53'' count=''6'' radix=''16'' > 00 08 05 54 02 65</i2c_write> <i2c_write addr=''0x53'' count=''6'' radix=''16'' > 00 0C 6E 64 61 FE</i2c_write>I hope this will solve the issue
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.