cancel
Showing results for 
Search instead for 
Did you mean: 

Looking for NFC/BLE P2P wearable

WarhogWearable
Associate

My partner and I are creating an app designed for P2P as well as traditional user/vendor interaction. We need a wearable that can create a mutual event on the back end when the two wearables touch or are in close proximity. I see the ST25R3916 or STM32 chips may be suitable but wondering if there’s already a wearable with these capabilities or if one can be designed/created that’s suitable for kids. I also see there’s a wearable - STEVAL-WESU1. Can the STM32 be used in the WESU1? I have additional requirements, like haptics, visual indicators, etc, that I can provide info on but I can’t find a wearable that can create a P2P event. Any help is appreciated

0 REPLIES 0