2025-09-04 5:29 PM
Hello,
I am planning to develop a small low-power wearable device using the STM32WB05KNV6TR.
My goal is to use the STM32WB05KNV6TR as a standalone MCU while implementing BLE communication.
From what I have found, this IC seems to be often used only for BLE communication, so I would like to clarify a few points:
Can the STM32WB05KNV6TR be used as an MCU that runs logic using peripherals such as ADC and SPI, while also handling BLE communication at the same time?
If it is possible, which development board would be suitable for testing the STM32WB05KNV6TR before hardware development?
I purchased the NUCLEO-WB05KZ board, but it seems to be in a module form (around 20x10 mm in size) instead of just the IC. Is this normal, or did I purchase the wrong version?
On the other hand, the IC on the STM32WB5MM-DK Discovery Kit looks like an appropriate size. Would this board be a good option to use?
Thank you in advance for your support.
Solved! Go to Solution.
2025-09-05 8:22 AM
Hello @bglglrr and welcome to the ST Community.
So, i suggest you migrate to the STM32WB05KZ if you want to use it as a standalone MCU and you have the NUCLEO-WB05KZ board that you can use it for MCU evaluation.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-05 8:22 AM
Hello @bglglrr and welcome to the ST Community.
So, i suggest you migrate to the STM32WB05KZ if you want to use it as a standalone MCU and you have the NUCLEO-WB05KZ board that you can use it for MCU evaluation.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.