2024-01-22 11:34 PM
according to datasheet I can set the RF field to High or Low via the MOSI pin, but when I look at the real RF field I found the problem that the RF field is set to Low and goes High immediately not remain low as ns delay time I set at firmware
Solved! Go to Solution.
2024-02-05 3:04 AM
Hello chaiwat,
can you provide further details what SPI commands you send. Could you send digital traces from your SPI communication ?
You could also have a look into the FW for more details how the PLL is configured, the power modes are set proper and the field is turned on or off. Please have a look to the file st25RU3993.c into the function void st25RU3993AntennaPower(uint8_t on) and the functions setting the various power down modes of the ST25RU3993 IC.
BR
2024-02-05 3:04 AM
Hello chaiwat,
can you provide further details what SPI commands you send. Could you send digital traces from your SPI communication ?
You could also have a look into the FW for more details how the PLL is configured, the power modes are set proper and the field is turned on or off. Please have a look to the file st25RU3993.c into the function void st25RU3993AntennaPower(uint8_t on) and the functions setting the various power down modes of the ST25RU3993 IC.
BR