2020-05-21 03:14 AM
Hello,
I'm using Nucleo 32f070RB and X-Nucleo 05a1 (st25r3911b).
At first, I started to itialize chip. I'm doing this with following the steps of "Power-up sequence" section in datasheet of st25r3911b, page 36.
There is my code
spiDirectComand(0xC1); // set chip to default
spiWrite(IO_CONFIGURATION_REG_1, 0x08); // just in case set 0x00h register to default 0x08
spiWrite(IO_CONFIGURATION_REG_2, 0x00); // just in case set 0x01h register to default 0x00
spiWrite(OPERATION_CONTROL_REG, 0x80); // Enable odcilator and regulator
HAL_Delay(100);
spiDirectComand(0xD6); // Direct command "Adjust Regulator"
HAL_Delay(100);
spiDirectComand(0xD8); // Direct command "Calibrate Antenna"
HAL_Delay(100);
test2 = spiRead(ANTENNA_CALIBRATION_TARGET_REG); // Just to check the value in the reg.
spiDirectComand(0xD9); // Direct command "Measure phase"
HAL_Delay(100);
Now I have one proglem and one question:
I'm new user of STM MCU devBoard and NFC technology, so I hope this is not stupid questions :)
Thank you for all the time spend for me,
Domen
Solved! Go to Solution.
2020-06-23 05:15 AM
Hi,
See https://community.st.com/s/question/0D53W000006G1H9SAK/how-to-start-with-st25r3911b-and-is-it-really-necessary-to-use-rfal-and-st25r3911-libraries-for-simpel-project which explain which files to use and how to setup the IRQ handler. In one of my latest responses, you will find a zip file (prilagoditevNFC) with a port on NUCLEO-F070RB. You can reuse this zip file as a basis. The STM32CubeMX ioc file is also included do that you can easily generate the code for your own IDE.
See then main.c and the demo.c for the proper usage of the RFAL api.
rgds
BT
2020-05-24 12:56 PM
Hi,
our X-CUBE-NFC5 package provides an NFC communication stack and a driver for ST25R3911B. This package supports NUCLEO-F401RE or NUCLEO-L476RG board but it can be easily ported on NUCLEO-F070RB. It includes chip initialization procedure and antenna calibration procedure.
Rgds
BT
2020-06-05 12:06 AM
Thank you for information.
Can you tell me how to check if direct command "Antenna tuning" was successfully executed?
I check Antenna calibration target register but nothing changed (before and after direct command executed).
All the best,
Domen
2020-06-05 12:59 AM
Hi Domen,
Calibrate antenna (D8h) is not an immediate command i.e. it starts a process of a certain duration and I_dct interrupt is triggered once the command is completed. Not waiting for the direct command completion interrupt (I_dct) is not a good practice.
As explained by @Ulysses HERNIOSUS in https://community.st.com/s/question/0D53W000006G1H9SAK/how-to-start-with-st25r3911b-and-is-it-really-necessary-to-use-rfal-and-st25r3911-libraries-for-simpel-project, if you prefer to write your own driver, observing the sequences and registers settings can be a good starting point. In the case of Antenna Calibration, see rfalCalibrate API in rfal_rfst25r3911.c and see the comment "Always run the command Calibrate Antenna twice".
Just for my own curiosity, why do you prefer to have your own driver?
Rgds
BT
2020-06-19 02:22 AM
I don't want to use the library because for my needs is too big and have too much of overhead.
Now I'm thinking to include library and then step-by-step start deleting unnecessary scripts and codes.
Rgds,
Domen
2020-06-19 04:43 AM
Hi Domen,
for your information, our code is scalable. For example, if only type 5 is used, you can configure RFAL_FEATURE_NFCA , RFAL_FEATURE_NFCB, RFAL_FEATURE_NFCF to false and significantly reduce the footprint.
Rgds
BT
2020-06-23 04:25 AM
Okay I will do this. I generate a new project with 32f070RB chip and set all the pins which needs to be set (comparing with your example). Now, I'm trying to import a library. Can you tell me which library is necessary to include for simple read/write project. Is It a "RFAL" or/and "ST25R3911" library?
One more question: After successfully included library I have a plan to start calling functions from library to initialize and all the other necessary function for correct working. Is this a correct procedure or you suggest different procedure?
Thanks a lot,
Domen
2020-06-23 05:15 AM
Hi,
See https://community.st.com/s/question/0D53W000006G1H9SAK/how-to-start-with-st25r3911b-and-is-it-really-necessary-to-use-rfal-and-st25r3911-libraries-for-simpel-project which explain which files to use and how to setup the IRQ handler. In one of my latest responses, you will find a zip file (prilagoditevNFC) with a port on NUCLEO-F070RB. You can reuse this zip file as a basis. The STM32CubeMX ioc file is also included do that you can easily generate the code for your own IDE.
See then main.c and the demo.c for the proper usage of the RFAL api.
rgds
BT