2023-05-30 1:44 AM
Dear Sir,
I am using the RFAL driver and I would like to achieve reading multiple ISO15693 tags. How can I obtain the UID of multiple tags with RFAL driver?
thank you very much in advance.
Best regards
Dai Sai
Solved! Go to Solution.
2023-06-06 5:28 AM
Hi Dai Sai,
yes, you could just change RFAL_NFC_MAX_DEVICES to a higher number.
But when going towards so many tags maybe the better approach is the mentioned rfalNfcvPollerSleepCollisionResolution() where user needs to provide the memory.
Best Regards, Ulysses
2023-06-12 3:40 AM
Dear Ulysses,
Thank you very much for your great help.
With your help, we realized multi tag access successfully. Up to 9 tags can be accessed in X-NUCLEO-NFC06A1 environment. I think 16 tags could be accessed in a larger antenna environment.
best regards
Dai Sai