2021-08-20 2:14 PM
Hi Experts,
Has anybody tried configuring the ST25R3916 in Card Emulation mode using external MCU using SPI bus ? I was looking for what register/s need/s modifications ?
Thank you for the help in advance.
regards.
Solved! Go to Solution.
2021-08-23 12:50 AM
Hi ASinh.2,
ST provides different SW packages with examples that demonstrate the Card Emulation feature. in particular, 2 demos are available in ST25 Embedded NFC library:
The examples are ready to run on NUCLEO-L476RG (STM32 MCU board) + X-NUCLEO-NFC06A1 (ST25R3916 expansion board) and can be easily ported to other MCU.
I would recommend to use the ST25 Embedded NFC library for your application.
Rgds
BT
2021-08-23 12:50 AM
Hi ASinh.2,
ST provides different SW packages with examples that demonstrate the Card Emulation feature. in particular, 2 demos are available in ST25 Embedded NFC library:
The examples are ready to run on NUCLEO-L476RG (STM32 MCU board) + X-NUCLEO-NFC06A1 (ST25R3916 expansion board) and can be easily ported to other MCU.
I would recommend to use the ST25 Embedded NFC library for your application.
Rgds
BT
2021-09-03 9:26 AM
Thanks Brian for the pointers. Will try the suggestions.
regards,
Anil