2023-11-01 1:06 AM
Just wondering if it's possible to add an extra sensor (SPI) on the STEVAL-SMARTAG1? Can the SPI sensor be replaced to complete the acquisition?
Solved! Go to Solution.
2023-12-05 8:48 AM
Hello there,
It is not recommended to modify the smartag board hardware. The traces and landing pads would not survive. Therefore, we prefer that you use the board AS-IS.
Best regards
2023-11-13 10:49 AM
Hello,
On STEVAL-SMARTAG1 there is no direct access to any SPI lines. Additionally, the only sensor that uses SPI interface is the LIS2DW12: it uses a 3-wire SPI where MISO and MOSI are connected together.
Hope this help. Best regards.
2023-11-13 5:59 PM
Yes, the sensor's circuit is i2c communication. But I want to use three-wire SPI communication to complete the sensor acquisition, what pin should I use to complete the circuit? Doesn't the figure below mean SPI communication?
2023-12-05 8:48 AM
Hello there,
It is not recommended to modify the smartag board hardware. The traces and landing pads would not survive. Therefore, we prefer that you use the board AS-IS.
Best regards