cancel
Showing results for 
Search instead for 
Did you mean: 

How can Sensors (SPI) be replaced?

Schuyler
Senior

Just wondering if it's possible to add an extra sensor (SPI) on the STEVAL-SMARTAG1? Can the SPI sensor be replaced to complete the acquisition?

1 ACCEPTED SOLUTION

Accepted Solutions
John TRAN
ST Employee

Hello there,

It is not recommended to modify the smartag board hardware. The traces and landing pads would not survive. Therefore, we prefer that you use the board AS-IS.

Best regards

 

View solution in original post

3 REPLIES 3
Michael GALIZZI
ST Employee

Hello,

On STEVAL-SMARTAG1 there is no direct access to any SPI lines. Additionally, the only sensor that uses SPI interface is the LIS2DW12: it uses a 3-wire SPI where MISO and MOSI are connected together.

Hope this help. Best regards.

Schuyler
Senior

Hi @Michael GALIZZI 

Yes, the sensor's circuit is i2c communication. But I want to use three-wire SPI communication to complete the sensor acquisition, what pin should I use to complete the circuit? Doesn't the figure below mean SPI communication?GB~A`(A0D$YU`GBWB(TDIIT.png

John TRAN
ST Employee

Hello there,

It is not recommended to modify the smartag board hardware. The traces and landing pads would not survive. Therefore, we prefer that you use the board AS-IS.

Best regards