2017-10-04 12:23 AM
do you have a easy product that can emulate nfc tag (like your tag) but with selected uid?
i don't want to deal with elctronic, i prefer somthing complete
thank you
#nfcSolved! Go to Solution.
2017-12-15 07:52 AM
The ST95HF is an integrated transceiver IC for contactless applications.
It supports ISO15693, ISO14443A & ISO14443B as RF Reader. In addition, it can be used as Tag emulation card for ISO14443A & ISO14443B.
See more information on our internet web site :
An evaluation board has been developped to demonstrate the main features of the ST95HF. About Tag Emulation feature, only ISO14443A has been developped.
Refers to EVAL-ST95HF board :
Best regards
2017-12-15 07:52 AM
The ST95HF is an integrated transceiver IC for contactless applications.
It supports ISO15693, ISO14443A & ISO14443B as RF Reader. In addition, it can be used as Tag emulation card for ISO14443A & ISO14443B.
See more information on our internet web site :
An evaluation board has been developped to demonstrate the main features of the ST95HF. About Tag Emulation feature, only ISO14443A has been developped.
Refers to EVAL-ST95HF board :
Best regards