cancel
Showing results for 
Search instead for 
Did you mean: 

is it possible to connect more than one RFDemo Board and use them asynchronously ?

Massimo Ponte
Associate
Posted on November 03, 2017 at 15:30

Hello, I'm using the RF Transceiver Demonstration Board, I connected it via USB, I successed in writing labview code that  read/write messages via NFC to a device.

My question is: is it possible to connect more than one Demo Board and use them asynchronously ? I need to read/write NFC messages at least to two devices at the same time.

Thank you

Regards.

Massimo Ponte

#m24lr-discovery
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on December 15, 2017 at 17:02

Hi Massimo,

If your question is about CR95HF-DEMO kit (embedded in the M24LR-DISCOVERY kit), it is not possible to use 2 readers via USB ports.

Best regards

View solution in original post

1 REPLY 1
Posted on December 15, 2017 at 17:02

Hi Massimo,

If your question is about CR95HF-DEMO kit (embedded in the M24LR-DISCOVERY kit), it is not possible to use 2 readers via USB ports.

Best regards