2019-04-01 11:32 PM
I evaluate ST25R3916 by using ST25R3916-DISCO kit and STSW-ST25R010.
In Antenna features tab, I confirmed AAT_A and AAT_B values changed for tuning when a piece of metal is approached to the antenna, but in poling tab, these value did not change when the metal piece is approached. Is this correct operation? I think the antenna is continuously tuned in poling mode. If it is wrong, please tell me when auto antenna tuning is used.
Solved! Go to Solution.
2019-04-10 11:46 PM
Hi
ad 1) Please see description of aat_en: The pins are driven to their value only when en=1 and aat_en=1. Otherwise they are weakly driven to some value.
ad 2) not sure what you mean: when en=1 and aat_en=1 then the AAT values are driven according to their corresponding register content. From SW side if they are not changed by the analog configs then they will keep their value.
ad 3) yes, see 1)
ad 4) We are working on an appnote which should be released in the coming weeks describing this problematic use-case.
Regards, Ulysses
2019-04-05 05:32 AM
Hi,
there are two features for competing for the AAT_A/B outputs. One is the analog config which switches the DACs according to the used operating mode and the tuning algorithm itself. We became aware of this issue and will make this more visible in upcoming versions of the software.
What you can do is:
Regards, Ulysses
2019-04-10 06:47 PM
Hi,
thanks for your answer. I confirmed AAT in poling mode.
I have additional questions,
2019-04-10 11:46 PM
Hi
ad 1) Please see description of aat_en: The pins are driven to their value only when en=1 and aat_en=1. Otherwise they are weakly driven to some value.
ad 2) not sure what you mean: when en=1 and aat_en=1 then the AAT values are driven according to their corresponding register content. From SW side if they are not changed by the analog configs then they will keep their value.
ad 3) yes, see 1)
ad 4) We are working on an appnote which should be released in the coming weeks describing this problematic use-case.
Regards, Ulysses