2025-03-17 2:53 AM - edited 2025-03-17 2:54 AM
I am making a board using your WLC38RX chip.
I had a problem during the experiment. When I applied a load and then disconnected it, the board rebooted.
So I found a solution. When I updated the Rx f/w, the reboot did not occur.
In order to find the parameter that affected it, I manually changed the config settings from the initial state without f/w update to the same as after the f/w update, but the board still rebooted.
I wonder why there is a difference when the Rx registers config settings are the same.
Is there an invisible setting value?
The f/w used is STEVAL-WLC38RX_config_1F46_EPP.memh.