2022-07-18 2:12 AM
Hello everybody,
I'm using the VNH9013 H-Bridge thermal sensor. Datasheet states on first page that thermal sensor coefficient is -8.1 mV/K, while on page 10 says -2 mV/K.
Any ideas on what is the right temperature coefficient?
Thanks in advance.
Solved! Go to Solution.
2022-07-18 5:53 AM
Welcome, @GEspo.2, to the community!
The temperature sensor in the VNH9013Y is realised by a diode, i.e. a pn junction. If a constant current is fed into such a pn junction, the resulting forward voltage has a temperature coefficient of -2mV/K. One can therefore assume a typing error on the first page.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
Regards
/Peter
2022-07-18 5:53 AM
Welcome, @GEspo.2, to the community!
The temperature sensor in the VNH9013Y is realised by a diode, i.e. a pn junction. If a constant current is fed into such a pn junction, the resulting forward voltage has a temperature coefficient of -2mV/K. One can therefore assume a typing error on the first page.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
Regards
/Peter