cancel
Showing results for 
Search instead for 
Did you mean: 

Viper26 power supply design

Kaleeswaran
Associate III

Hi, 

 anyone tells me how to design a 24vdc to 15vdc  buck converter using viper26ld?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

If you want to stay with STMicroelectronics, there are a bunch of devices for converting 24V to 15V, the recommendation only depends on the output current. You could e.g. have a look at theL6981 or the L6986 .

Regards /Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
AScha.3
Super User

hi,

you have 24V IN ? and want 15v out ? then viper26 is totally wrong for this.

take a LV2862XLVDDCR or TPS563300DRLR ; which current ??

If you feel a post has answered your question, please click "Accept as Solution".

   Thank you for your reply

  Current 400mA

Peter BENSCH
ST Employee

If you want to stay with STMicroelectronics, there are a bunch of devices for converting 24V to 15V, the recommendation only depends on the output current. You could e.g. have a look at theL6981 or the L6986 .

Regards /Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

or cheaper and also STM : the good old MC34063 . ->

MC34063ABD-TR .

 

at mouser :  511-MC34063ABD-TR

If you feel a post has answered your question, please click "Accept as Solution".

The MC34063 is a very old device working with very low switching frequency, which requires bulky passive devices. In addition it is an asynchronous regulator, which requires a Schottky diode. All in all this might be the more expensive and bigger solution.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you for your suggestion.