cancel
Showing results for 
Search instead for 
Did you mean: 

Viper Zero Dual Output Standby SMPS

SShah.8
Associate

Hello

I am in the design/prototype stage of standby SMPS, specifications are below

Input range: 85VAC to 265VAC

Output-1: 12V 0.150A

Output-2: 18V 0.150A

Output 1 will be the output on the secondary side

Output 2 will be on the PRIMARY circuit side feeding ANOTHER SMPS circuit, and the GND of that output will be connected to the main GND of the main SMPS.

In another word, output 2 will be the main power source to power the MAIN SMPS.

I tried to make a design with the tool found on the site, but I never got the transformer winding details or the transformer winding method to send to the manufacturer, like what you can get in Power Expert designer.

I also don't want to face surprises with audible transformer noise!

The SMPS must NOT draw more than 0.3W in standby and in no-load conditions

Any suggestions?

0 REPLIES 0