cancel
Showing results for 
Search instead for 
Did you mean: 

Viper comp design

Mnemonic
Associate III

Hello everybody,

I need to user Viper115HS or Viper222XS vith 15V 600mA output at non isolated buck topology. I was designed my Fb pin with 130K Ohm and 11K Ohm resistors. But I can not find right Comp pin configuration. could you write capasitor and resistor configuraton for 15V 600mA output

3 REPLIES 3
AScha.3
Chief II

Hi,

always same questions...?

1. you could use, what eDesign suite telling :  (for 400mA max.)

AScha3_0-1718348934969.png

2. 600mA not possible with non-iso buck ; 590mA would be absolute maximum. But "critical" design.

3. Use a transformer (as almost everybody...) and it will work . (If you have the matching transformer ! )

If you feel a post has answered your question, please click "Accept as Solution".
Mnemonic
Associate III

I can not calculate for 590mA at e-design. could you share

Me too.. just maximum possible message there. Not yet calculation.

 

 

If you feel a post has answered your question, please click "Accept as Solution".