cancel
Showing results for 
Search instead for 
Did you mean: 

Using X-NUCLEO-IHM01A1 without an STM32 Nucleo board

dvelasco
Associate II
Posted on February 11, 2015 at 22:42

I'm trying to use an X-NUCLEO-IHM01A1, but without an STM32 board. That is, I need to wire up each of the necessary pins individually, sending the proper signals via another microcontroller.

For now, I just need to get to the point at which the board powers up and the green D7 LED comes on.  What steps do I need to perform?  I applied 3.3V to the IOREF pin on CN6 and I tied the the /RST pin on CN5 to 3.3V.  Are these steps correct, and what else do I need to do?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0