cancel
Showing results for 
Search instead for 
Did you mean: 

The opto coupler fails frequently in the circuit below.

DIGIPRESSURE
Associate II

hello.
I am using bta16-800-bw for 400v 3 phase motor phase control.
In triac control, the optocoupler frequently fails in the circuit below.
For couplers, use moc3071sm, il4208-x007, etc.
Please see photos for symptoms.

I'm thinking of changing to BTA16-800CW.
I'm asking for advice.

and!
bta16-800-bw Snubless type.
Should I install another snubber circuit like the circuit?
Or is it okay not to use a snubber circuit in the triac?
C14, C15, R8, and R9 you pointed out are snubber circuits, and C is the X-cap.

There were cases where this snubber resistor was damaged or burned.
I would like to ask for advice on two phenomena.

 

출력스위치 정상출력.jpg출력스위치 +측 출력  특성불량현상2.jpg출력스위치 단방향출력  불량현상1.jpgThe picture on the oscilloscope shows line T + fan W of the circuit tested with a differential probe.MOC3071_Circuit.png

1 ACCEPTED SOLUTION

Accepted Solutions

I am using bta16-800-bw for 400v 3 phase motor phase control.
In triac control, the optocoupler frequently fails in the circuit below.
For couplers, use moc3071sm, il4208-x007, etc.
Please see photos for symptoms.

I'm thinking of changing to BTA16-800CW.
I'm asking for advice.

and!
bta16-800-bw Snubless type.
Should I install another snubber circuit like the circuit?
Or is it okay not to use a snubber circuit in the triac?
C14, C15, R8, and R9 you pointed out are snubber circuits, and C is the X-cap.

There were cases where this snubber resistor was damaged or burned.
I would like to ask for advice on two phenomena.

The picture on the oscilloscope shows line T + fan W of the circuit tested with a differential probe.

View solution in original post

4 REPLIES 4
Peter BENSCH
ST Employee

To get answers from the English-speaking community, it is helpful to ask in English as well. I have therefore translated your text using a web-based tool:

Hello.
I am using a BTA380-3BW for phase control of a 16V 800 phase motor.
The optocoupler fails frequently in the circuit below.
I use MOC3071SM, IL4208-X007, etc.
See the photo for symptoms.

I am thinking of changing to BTA15-800CW.
Looking for advice.

Second!
Is it ok to not use the snubber circuit in a triac without a snubber? The snubber is built into the circuit separately.

There are times when this snubber resistor breaks or burns out.

The photo of the oscilloscope shows line T + fan W in the circuit tested with a differential probe.

I would like to enquire why you are asking in the community of STMicroelectronics if BTA380-3BW, BTA15-800CW and the optotriacs are not devices from STMicroelectronics?

Nevertheless, I'd like to give you a hint: you probably inserted C14 and C15 to realise a capacitive voltage divider, right? Have you taken into account that the capacitors cause a phase shift?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AScha.3
Chief II

Hi,

1. write in English.

2. try the standard circuit : from ds ->

AScha3_0-1715161061927.png

R = VPAC / ITSM

 

 

If you feel a post has answered your question, please click "Accept as Solution".

hello.
I am using bta16-800-bw for 400v 3 phase motor phase control.
In triac control, the optocoupler frequently fails in the circuit below.
For couplers, use moc3071sm, il4208-x007, etc.
Please see photos for symptoms.

I'm thinking of changing to BTA16-800CW.
I'm asking for advice.

and!
bta16-800-bw Snubless type.
Should I install another snubber circuit like the circuit?
Or is it okay not to use a snubber circuit in the triac?
C14, C15, R8, and R9 you pointed out are snubber circuits, and C is the X-cap.

There were cases where this snubber resistor was damaged or burned.
I would like to ask for advice on two phenomena.

The picture on the oscilloscope shows line T + fan W of the circuit tested with a differential probe.

I am using bta16-800-bw for 400v 3 phase motor phase control.
In triac control, the optocoupler frequently fails in the circuit below.
For couplers, use moc3071sm, il4208-x007, etc.
Please see photos for symptoms.

I'm thinking of changing to BTA16-800CW.
I'm asking for advice.

and!
bta16-800-bw Snubless type.
Should I install another snubber circuit like the circuit?
Or is it okay not to use a snubber circuit in the triac?
C14, C15, R8, and R9 you pointed out are snubber circuits, and C is the X-cap.

There were cases where this snubber resistor was damaged or burned.
I would like to ask for advice on two phenomena.

The picture on the oscilloscope shows line T + fan W of the circuit tested with a differential probe.