2021-09-21 02:21 PM
I know that the STPMIC1C is the "custom" version of this PMIC. And long term, we may choose to use that version. But, due to availability, we want to create our reference design with the STPMIC1E which we can acquire ~300 parts for our prototype build. Then in mass production, we'd likely switch to the STPMIC1C. We have no problem programming the NVM as long as the values stay present on subsequent power-ups.
Specifically, we'd like to program:
BUCK1 to 0.8V
BUCK2 to 1.1V (default)
BUCK3 to 1.8V
BUCK4 to 0.65V
Thanks.
Tom
Solved! Go to Solution.
2021-09-21 10:42 PM
Welcome, @TWarn.1, to the community!
Yes, all pre-programmed STPMIC1 can be changed to other output voltages of the Buck regulators and LDOs, which is possible up to 1000 times thanks to the included NVM. You'll find some description in the datasheet of the STPMIC1, section 5.5.2:
The NVM is composed of 64 bits customizable parameters (accessible from shadow registers):
BUCKs and LDOs regulators:
[...]
NVM read operation is performed automatically before each POWER_UP sequence to set control registers with default values and configure POWER_UP and POWER_DOWN sequence.
NVM write operation can be performed several times at product level to:
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-09-21 10:42 PM
Welcome, @TWarn.1, to the community!
Yes, all pre-programmed STPMIC1 can be changed to other output voltages of the Buck regulators and LDOs, which is possible up to 1000 times thanks to the included NVM. You'll find some description in the datasheet of the STPMIC1, section 5.5.2:
The NVM is composed of 64 bits customizable parameters (accessible from shadow registers):
BUCKs and LDOs regulators:
[...]
NVM read operation is performed automatically before each POWER_UP sequence to set control registers with default values and configure POWER_UP and POWER_DOWN sequence.
NVM write operation can be performed several times at product level to:
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter