cancel
Showing results for 
Search instead for 
Did you mean: 

STPM32 IEC accuracy class reference

Franco Zampicinini
Associate II

Dear all, on STPM32 datasheet (DS10272 - Rev 12 ) there is this statement: "a meter using the STPM3x can reach IEC class 0.2 accuracy". On IEC standard, for meters, I only found class 0.2s specifications, where class 0.2 is only applied to current transformer. Please can you give me the IEC reference cited? Thanks in advance.

1 ACCEPTED SOLUTION

Accepted Solutions

Hello! the datasheet in fact refers to Class 0.2 S of IEC 62053-22.

Best regards

Marilena

View solution in original post

5 REPLIES 5

Hello! the datasheet in fact refers to Class 0.2 S of IEC 62053-22.

Best regards

Marilena

Hi, many thanks! I wonder is you are able to add these information on the datasheet. Kind regards,

It is among the features in the first page, referred as IEC 62053-2x.

Best regards

Marilena

Got it. Maybe class 0.2s could help to avoid misunderstanding.

Thanks again.

Buon lavoro!

Thanks! we will add in the next datasheet release.

Buon lavoro!

Marilena