2011-12-07 01:34 AM
Hello
I am using''
ACIM
and
BLDC
motor control
firmware
library
V1.0''
BLDC
motor
and
a
hall
sensor.
In closed
loop
speed when
the motor
decelerates
the system reduces the
duty cycle.
Finally,
there is no
PWM
signal
and the motor
slows down
freely.
Is
the library
prepared
to stop
the motor
in closed loop (
Four-Quadrant)?Best regards
2011-12-09 08:29 AM
In the STM8 BLDC libary is implemented an active brake strategy injecting a DC current in the motor. It is done imposing a prefedined power switch configuration like the one of the alignment phase with a modulated PWM and can be enabled using the GUI.
Ciao Gigi2011-12-12 01:42 AM
Thank you for answering
so quickly.
best regards