cancel
Showing results for 
Search instead for 
Did you mean: 

STLQ020 reverse protection diode?

CptSlow
Associate

I'm working on a low-power design and planning to use a STLQ020. The datasheet doesn't mention the need for a protection diode, nor does it mention that there is one integrated..

Is there an integrated protection diode?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Well, the data sheet does not mention a protection diode, but it does mention in the absolute max ratings: Voutmax = -0.3V ... Vin+0.3V. This means that with e.g. input = 0V, a possible voltage at the output must be limited to 0.3V, e.g. with a Schottky diode from Vo to Vi.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Well, the data sheet does not mention a protection diode, but it does mention in the absolute max ratings: Voutmax = -0.3V ... Vin+0.3V. This means that with e.g. input = 0V, a possible voltage at the output must be limited to 0.3V, e.g. with a Schottky diode from Vo to Vi.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.