cancel
Showing results for 
Search instead for 
Did you mean: 

STGIB10CH60TS-L Isolation Issue

Hasan06
Associate II

Hasan06_0-1744009471564.png

Hello, would it cause any issues if 'PWR_GND' (highlighted in green) and 'SGN_GND' (highlighted in pink) are not referenced to the same ground?

Thank you in advance. Best regards.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @Hasan06, to the community!

yes, 'PWR_GND' and 'SGN_GND' must be galvanically connected to the same GND. But of course, these two GNDs must be separated from each other as much as possible in terms of high frequency by a suitable layout so that no ground bouncing occurs on the input side due to the large ripple currents on the power side. For an example of how something like this can be done, you can take a look at the GERBER layout of the STEVAL-IPM10B.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @Hasan06, to the community!

yes, 'PWR_GND' and 'SGN_GND' must be galvanically connected to the same GND. But of course, these two GNDs must be separated from each other as much as possible in terms of high frequency by a suitable layout so that no ground bouncing occurs on the input side due to the large ripple currents on the power side. For an example of how something like this can be done, you can take a look at the GERBER layout of the STEVAL-IPM10B.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Hasan06
Associate II

Thank you so much, dear Peter.