Skip to main content
Associate
January 20, 2025
Solved

STEVAL-WBC86TX Coil change

  • January 20, 2025
  • 2 replies
  • 763 views

Hello everyone, I am working on a wireless charger based on the STEVAL-WBC86TX, but we cannot find availability for the transmitter coil reference 760308111 among its components. We would like to know which other references would be compatible with the STWBC86 chip. Thank you for your attention.

This topic has been closed for replies.
Best answer by Didier HERROUIN

As an alternative to the original coil, you can look for a coil which is compliant to MP-A11 profile, defined by the Qi standard. It should allow you to charge off-the-shelf receivers up to 5W with the STWBC86 platform. 
The MPA11 has been defined as a 6.3µH coil with following parameters :

  • Outer length : 44m
  • Inner length : 20.5 mm
  • Thickness : 2.1 mm
  • Number of turns per layer : 10 (5 bifilar turns)
  • Number of layers : 1 or 2

Best regards,

Didier

2 replies

Didier HERROUIN
Didier HERROUINBest answer
ST Technical Moderator
January 21, 2025

As an alternative to the original coil, you can look for a coil which is compliant to MP-A11 profile, defined by the Qi standard. It should allow you to charge off-the-shelf receivers up to 5W with the STWBC86 platform. 
The MPA11 has been defined as a 6.3µH coil with following parameters :

  • Outer length : 44m
  • Inner length : 20.5 mm
  • Thickness : 2.1 mm
  • Number of turns per layer : 10 (5 bifilar turns)
  • Number of layers : 1 or 2

Best regards,

Didier

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
ST Technical Moderator
January 22, 2025
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.