2017-01-10 01:59 AM
Hello!
Has anyone worked with the STEVAL-ISW001V1 demoboard or has designed an inverter welder based on the demoboard schematics? My design is working well in normal operation but I have some issues with the short-circuit condition and I need an expert to ask some questions...
Thanks,
Markus
2017-10-24 04:05 AM
Yes i was working on this with
. Short circuits should working fine, try to do it on the next stage.