2020-12-26 1:09 AM
Hello, please help me understand:
1) What will happen if IN voltage less than the battery voltage? What voltage will in SYS in this case?
2) Сan I connect SYS pin to IN? I'ts safe?
2020-12-28 7:27 PM
1) shall not happen
Battery floating voltage is adjustable up to 4.45 V.
The minimum Vin will be 4.75 V when Vfloat is set to 4.45 V.
2) take your own risks
It means to skip the protections within STBC03.
2020-12-29 1:28 AM
Thanks for the answer. Can you please clarify one more question:
What if the battery is fully charged (4.2 V) and we supply 4.2 V or less( for example, 3.9 V) to the IN pin. In this case, what will be the voltage on the SYS pin?
2020-12-30 7:57 PM
It will not work.
There is no grantee outside the range of operating input voltage : 4.45 V to 5.4 V
2024-02-17 7:43 AM
Hello,
We could use STBC3 for stand alone application. I want to charge a mini battery as below specification.
I am planing to draw a pcb that contains USB socket and its power will be come from 5V phone charger. May I use the STBC3 stand alone to charge this battery or should i put mcu to control charger limits. I confused. Previously I use TP4056 IC to chage higher capacity. It is the first time i am going to charge such a lower batter. May you give some advise to me.
Best regards.