2025-09-18 10:13 PM
@TDK , @Peter BENSCH we are facing SPV1040 IC failure (burns) in the field, after around 3 months of installation, attached schematic and our solar Panel speciation Voc:4.55V, Vm:3.85V, ISC:1026mA, Im:950mA.
Battery spec - 9000mAh, 4.2V Lithium ion.
2025-09-19 2:01 AM
Welcome @MANIPILLAI, to the community!
It looks like you based your design on the STEVAL-ISV012V1. However, if all components are assembled as shown in your schematics, you have at least one error: R35 is 82k in your design, which causes the SPV1040 to try to generate an output voltage of 34.79V (VCTRL is compared to 1.25V). So if you actually have 82k on the board, that could be the explanation and you should replace it with 820k.
Hope that helps?
Regards
/Peter
2025-09-19 2:10 AM
Thanks for your quick response.
sorry it's a typo error in schematic, actually we are using 820k in our assembled boards also all the other components are assembled as per schematic.
2025-09-19 2:35 AM
OK, the next possible fault is the boost coil, whose maximum saturation current is somewhat low. It is possible that the peak current exceeds the saturation current limit when the solar panel is poorly lit, i.e. when the input voltage is low, causing the inductance to collapse and suddenly become a short circuit. You could therefore test a boost coil with a higher saturation current.
If this is not the cause, the defective SPV1040 would need to be analysed more closely to determine the possible causes.
Regards
/Peter
2025-09-19 2:46 AM
Thanks for your quick response.
we will test with replacing the boost coil, can you please suggest any spec for it.
regarding defective SPV1040, we found short with Lx and GND.
2025-09-19 4:12 AM
The short between LX and GND confirms my suspicion that the boost coil may be undersized. Its magnetic field collapses while the boost transistor is switched on, causing a short circuit between the solar panel and GND, which will overload / kill the boost transistor.
I recommend a coil with a minimum saturation current of 4A, but this will probably be bulkier because the coil wire is thicker.
Regards
/Peter
2025-09-29 5:51 AM
@Peter BENSCH we are tested bellow part number,
https://www.digikey.in/en/products/detail/w%C3%BCrth-elektronik/74404084100/4865710
After replaced L1 inductor from 1.69A saturation current into 4.5A saturation current we are not seen the SPV1040 failure still now. We are continuously monitoring that later we will update you. In addition, we are conducted with solar panel with SPV1040 setup we found it battery charge current is less than of input current. Please review the test report as in attachment. Please give the guidelines to achieve more charge current to the battery
2025-09-29 11:46 PM
@Peter BENSCHBENSCH we are waiting your reply
2025-10-07 9:57 PM
we are waiting your reply
2025-10-13 11:43 AM
Your statement that the battery charging current is lower than the input current is entirely correct, as the SPV1040 operates as a boost converter and the efficiencies of the SPV1040 and the L6924D must also be taken into account.
I see that you still have an unanswered question: you would like to achieve a higher charging current, correct?
You have already set the maximum charging current to 974mA with Rprg = 12k. However, if the SPV1040 does not provide enough power, the L6924D cannot supply this current. You would therefore also need to optimise the output power of the SPV1040.
Please remove your R29 and load Vrs+ with a suitable ohmic load resistor so that you can determine the output power. Please also double check the MPPT settings of the SPV1040.
Regards
/Peter